This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Drv8301 speed controller module

Other Parts Discussed in Thread: MOTORWARE

Hello,

I have a board driver 8301 and a controlCARD. On the driver, there are a module "Speed controller" where we can change the speed manually and the buttons "start", "stop". It seems that the controlCARD will read the signals from this module through ADC and generate the speed for motor. I read the documents in Motorware and the code examples, but I cant find out the manual for this function.If someone has experiences in this case, can you tell me about it ?

Best regards

  • Hi Maxime,

    Right now the existing projects do not use these as inputs.

    You would have to modify the firmware appropriately to take an action based off inputs from these.

    I would recommend posting to the C2000 InstaSPIN forum if you have more in depth questions.