This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10983 EVM: Problem driving a blower motor

Other Parts Discussed in Thread: DRV10983

Dear TI Team Member,

My name is Rick Casler and I am the VP of Engineering at Grabit Inc., a start-up in Silicon Valley.  Grabit is developing robotic assembly systems.  We are evaluating the DRV10983 BLDC Driver IC for use in a blower control application.  To that end, we purchased and just received a DRV10983 EVM (EVM).  I got it running this morning, out-of-the-box.  The EVM circuit board drove a motor that came with the Evaluation Module.  

This afternoon I connected the Grabit Blower to the EVM.  I followed the tuning instructions in Sections 4.1-4.8 of the DRV10983 Tuning Guide Rev C.  I set a speed of 100 and the blower did not spin as expected.  I backtracked and reloaded the GUI and successfully drove the EVM motor to confirm that the EVM Board was still working.  I set it up again to drive the blower and again, the blower did not spin.

The Blower is a three-phase motor with a resistance of about 80 milli-ohms and a voltage constant of 2.3 mV/Hz.  Per the above, I followed all of the other configuration steps in the Tuning Guide but to no avail.  The blower does not rotate, not even a little bit. 

I need help at your earliest convenience.  Please advise next steps.

r

  • Hi Rick,

    Our experts have been contacted and should reply soon.

    Thank you for the details. Can you also provide the system voltage you are using?
  • Rick,

    Hope you are following the Tuning Guide to tune your motor.  www.ti.com/.../slou395c.pdf 

    You mentioned your motor velocity constant to be of 2.3mV/Hz , that is extremely low. For Blowers kind of application, these values are expected to be low only but this is still lower. 

    If the operating voltage is 12V , with this kind of velocity constant, you will be expecting to spin the motor more than 5kHz electrical speed. Is that correct ? If 5kHz electrical is what your requirement is, it is difficult to spin the motor with DRV10983, One thing you can try is to double the PWM frequency where we can get more samples to work with. 

    Thanks,

    Jasraj