Other Parts Discussed in Thread: DRV8308
Hi,
I can drive the motor included in the package with DRV8308EVM. However, as soon as I connect the DF45 Nanotec BLDC Motor to the evaluation board, I see some problems. According to the motor datasheet, he internal windings of the motor are STAR and not DELTA and Hall sensor feedbacks are not inverted.
My connections are as below.
U/V/W Gray/Brown/Yellow
Sensor Power Red/Black
Hall.U/V/W+ Blue/Green/White
Motor cannot rotate properly in both modes and just shakes at a position. FGOUT is okay while spinning by hand with 0% PWM command and enabled. But when I exchange V+ and W+ Hall sensor feedbacks, the rotation will be good in just one direction while setting HALLPOL to 1 (!) and in the reverse rotation direction the spinning is not smooth. Of course the motor datasheet says that pulses are not inverted.
Would anyone please give me some help on connections and parameter settings. Specially if ADVANCE is needed in STAR configuration. Thanks in advance.