This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8830 I2C motor driver

Other Parts Discussed in Thread: DRV8806, DRV8846

Dear Sir 

I would like to find I2C interface and support 12Vin / Iout =500mA for 4 channel stepper motor (don;t need micro step)

I saw DRV8806 have 4 channel output ,but seems like serial interface is not the same with I2C

Could you have to suggest 4channel I2C motor driver 

Thanks

  • Hi Kai,

    Unfortunately, we do not have a device that has meets your stated requirements.

    Can you provide more information on the application? Why is an I2C interface requested?

    If you don't need the I2C interface, the DRV8846 is a fit. The device has a STEP/DIR interface which is commonly used.