I am having some troubles with the DRV8402. I am using it to drive a very low inductance pancake motor, and have the switching frequency set at 200khz. The first time, the part worked fairly well, until I started to place a load on the motor. The current hit about 3 amps, and the DRV8402 failed, and pulls down the 24v supply. The second DRV8402 failed after 10 seconds with no load on the motor, and exhibited the same problem. The documentation indicates that external snubber diodes are not needed, but should they be added?