This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Robotics BLDC Motor Driver Questions

Other Parts Discussed in Thread: DRV8301, LAUNCHXL-F28069M, BOOSTXL-DRV8301

Hey, I'm looking to drive a BLDC motor for a small robotics application, but I have a few questions before I proceed forward on this project. The application I am intending this for needs to use two motors that will be driven at different speeds and at low speeds about 1 RPM or less. For an application going this slow will I need to have a motor that provides feedback with hall sensors or rotary encoders? I also need the motors to change direction, velocity very quickly and accurately.  I have been looking into TI's technology like InstaSPIN-FOC and InstaSPIN-Motion, would I be able to control the motors with these technologies? Also what would be a good motor driver and motor pair? I've been looking into the DRV8301 with its EVM BOOSTXL and the LAUNCHXL-F28069M controlling it, would these be good solutions?