dear ladies and gentlemen,
for my DC Motor I need a higher Supply Voltage than the DRV8701 withstand.
The N-Fet output stage needs more Current for Charge than the DRV8701 can deliver.
Is it possible to connect 2 Half Bridge Driver e.g. LM5109B between the DRV8701 and the 4 N-MOSFETs?
The DRV8701 should only control the ON/OFF sequence of the FETs and the LM5109B should drive the
N-FETs with the right Current and Voltage.
Could I disable the charge pump of the DRV8701, so that the Output of Low-Side has the same Voltage Level than the High Side?
Thanks in advance
Thomas Straßer