Other Parts Discussed in Thread: DRV8833C
DRV8833C Evaluation Module 1. On the datasheet, it says If external control of the DRV8833C is desired, remove R11 to isolate the MCU from the DRV8833C. I'm currently using an external MCU, how do I remove the R11 on this evaluation board.
2. I would like to use an external MCU to control the nSleep mode with a GPIO, is there a connection point on this eval board for me to use a jumper wire to connect my external MCU breakout board?
3. I'm currently supplying the voltage 5 V to this DRV8833C Evaluation Module using one of the 5V pin on the MCU breakout board, when I try to connect the whole setup to the laptop using a USB cable, the laptop gives a message saying the USB device has exceeded the power limit, I don't quite understand why this would happen, as the motor driver can be supplied between 1.8-10 V, and I'm giving it 5V now. Please help and explain this.