This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Help me find the suitable motor driver for BLDC servo application

Other Parts Discussed in Thread: DRV10983, DRV8307, DRV8308, DRV10970

Hi Everyone,

I am looking for a motor driver IC to control a 1A 24 V BLDC motor (control input - Analog/PWM). I have couple of questions;

1. Does TI have any motor driver IC which provides Sinusoidal commutation using Hall sensor signals?

2. If the answer to the above question is "NO", which are the recommended motor driver ICs that provide sinusoidal commutation feature for this specification of motor?

Thank you,

Vivek