This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Dual-stator dual winding permanent magnet synchnous generator, on this process in some state i want to design a circuit with following requements::

Other Parts Discussed in Thread: DRV8312

heloo all, i am working on Dual-stator dual winding permanent magnet synchnous generator, on this process in some state i want to design a circuit  with following requements::

1)input will in range of 3v to 6v   and want output will be voltage of (6v to 8V ) and  10watt ,max power required.( circuit )

2) for the same circuit i was suppose to give an PWM signal as input.( this will be generated by reference singal and hall effect sensors deference)

3)according to the input PWM signal it should control the control winding speed.

 for this what circuit or ic's i was suppose to use.