This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSC2013EVM Motor

Other Parts Discussed in Thread: DRV2605

Hi,

One of my customer purchased TSC2013EVM

The user manual of the above EVM includes BOM. BOM lists LRA Motor with part no AAC1030.

But customer didn't receive the above motor. Kindly help whether the EVM comes with motor.

Also user manual says "an LRA motor is attached as an actuator" what does it mean?

  • Hi Dinesh,

    It looks like this thread was accidentally posted in the wrong forum. To ensure you continue to get the best support for the DRV2605, I've moved your thread into the Haptics Forum.

    In the meantime, take a look at the picture of the TSC2013EVM shown on one of our distributor's websites. If you look at the bottom right of the board where it says "Haptics", it seems like the LRA is not included with the EVM but would be connected there. Since the LRA would be application- and customer-specific (such as size requirements), I'm assuming that's why it's not included. Our Haptics experts should be able to provide more insight here.

    Regards,

    James

    MSP Customer Applications

  • Sorry Dinesh, the BOM should actually refer to a jumper/header that a LRA motor can be plugged into. I will look into getting the BOM fixed to accurately reflect what is shipped with the EVM. Do you need assistance in finding a LRA for your application?

    Regards,

    Kelly Griffin