Hello,
I am using the DRV8432 set to parallel mode as a TEC driver. Rather than using PWM to control TEC drive, we are varying the input voltage (PVDD). The PWMA and PWMB inputs are used to flip the polarity of the TEC from heating to cooling. I am seeing some odd behavior from the DRV8432, in that after a few seconds of operation, the output will start to pulse. It won't go completely off, though - if, for example, I am supplying 24V, the output will switch between 24V and 5V at anywhere from a 0.5-3Hz rate. There are no fault indications (pins 2 and 3 are high), and the PWM and reset control inputs are steady. Temperature is not an issue - the heatsinks attached to the DRV8432 are maybe 10C above ambient.
Is there an issue with using the DRV8432 as a straight DC driver? My intended application is to switch the polarity across the TEC with a variable drive voltage of 0-24VDC. I understand that there will be some short pulses on the output as the bootstrap caps are charged, but I would think that that would be barely perceptible - not the slow pulsing I am seeing.
Any thoughts?
Thanks!!
-Mike