I'm attempting to use the DRV8662EVM. Unfortunately, it either isn't delivering what the spec says it should deliver, or I'm doing something wrong. I suspect the latter..
Anyway, I want to use the DRV8662 to amplify my Piezo Transducer to give it a 50v peak to peak waveform at 25khz.
So, to test this out, I got the DRV8662EVM and am trying to get it to do the above.
I applied 4.65vdc to the VBATT terminals. The 'Active' light flashes. I power off and connect my Piezo directly to the + and - pins on the OUT terminal.
Power on and active light blinks again.
Power down
I built a first order filter using the schematic in the UserGuide and connected it between my PWM and the EXTIN pins
I also removed JP2 and 3 as per the User Guide Instructions.
Power on and press the "TRIG" button 1 time to enter mode 2 which has External Signal Enabled, and Gain 0 and 1 both disabled. LEDs have Active solid ON and both Gain LEDs off.
Apply power again and get pretty much nothing from the OUT terminals. I would have expected a 50v amplification of my PWM waveform at 25khz, but I get noise.
I tested my input waveform with an oscilloscope. It is accurately showing a square wave at 25khz with -3 to +3 peak to peak voltage.
I tested waveform coming out of the First Order Filter. It's barely measurable, but is a weak sign wave at about 25khz.
I then removed the first order filter and attached my PWM signal directly to the EXTIN pins. At this point, I DO get a visible signal, however, it is not amplified. In fact, the signal coming out of the OUT pins is weaker than what is going into the EXTIN pins.
My Piezo has a capacitance of 2500pF.
Any ideas why the DRV8662EVM isn't amplifying my signal and BOOSTING my voltage through the piezo? Can the DRV8662 be used to amplify a PWM signal?
Thanks