We're developing a new product that will use the DRV2605.
We've been using the DRV2605EVM-CT demo board for initial tests and now we were planning on using the DRV2605EVM-BT demo board mounted on a wrist strap for field testing.
However, we have run into a problem. TI seems to have orphaned the -BT demo board and perhaps also the chips on it.
The -BT board comes with code and with an iPhone app. The app doesn't work, the code won't compile and it appears that TI hasn't published a fix since they were made aware of the problem months ago!
If the DRV2605EVM-BT is no longer supported we will have to lay out a circuit board in order to go forward as the -CT demo board is too large for field testing.
Has TI indeed dropped support for the -BT board? It's not an old board and there are still units in distribution!
Also, and at this point more import: Will TI support the -CT board and the critical chips on it (MSP430G2x53/MSP430G2x13 and DRV2605) ?