This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using DRV 2605 or similar chips to drive multiple LRA actuators

Other Parts Discussed in Thread: DRV2625, DRV2605, DRV2605LEVM-MD, DRV2605L

Hello E2E forum,

I am working a University project where we would like to use 6 to 8 LRA actuators to create haptic feedback. I found the DRV 2605 chip as a potential solution for driving these LRA motors. My question is whether there is a single chip that can drive multiple actuators (using the Immersion Touchsense 2200 software that has the audio-to-vibe features and that is lisenced to the DRV 2605, for example) or if using multiple DRV 2605 chips is the way to address the issue.

Thanks for your help

  • Hello Allan,

    The DRV2605 measures the back-EMF when driving any given actuator in order to run the Automatic Level Calibration. Connecting more than one actuator may create some interference in terms of more than one back-EMF will be connected in parallel as seen from the device. We have tested driving up to 2 LRA actuators using a single device (DRV2625), in open-loop mode, and obtained good results. However, I would imangine things would get complicated connecting those 6 to 8.

    I you want to go ahead and try it, make sure your power supply can provide enough current.

    Our DRV2605LEVM-MD drives up to 8 LRAS using 8 different devices, so I would recommend you give that a look.

    Please, let me know if you have any further questions,
    Leo
  • Hi Leo, thanks for your help. I have a couple of follow up questions for you. For the DRV2605LEVM-MD, which type of connection is that for the 8 device attachments? Also, can you control the intensity of the vibrations in the audio-to-vibe mode in a way that is independent of the volume of the audio itself? Moreover, what types of vibration modes does audio-to-vibe offer?
  • Hi, Alan:

    the 8 DRV2605Ls are connected to MCU via I2C switch.

    each DRV2605L can be controlled independently.

    but Audio-to-Vibe vibration is tightly related to the audio volume. this is a technology from Immersion.