Other Parts Discussed in Thread: DRV8811
Hello,
I am using DRV8811 to control a motor. I am applying 3.3V to STEP pin for 50us and 0V for 9ms. After some revolutions of motor the DRV getting too hot, it stops the motor like glitches. I have copied the schematic from DRV8811's datasheet. I am revolving motor in full step mode. With such slow rotating speed there is a more heating problem.
Some details are mentioned below-:
Motor type-:bipolar
step angle-:1.8 degree.
current rating-: 1.5A
Vm is 11.57v
Vref=1.65V
VDecay=1.65V,