This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OCP DRV8871 VS OCP DRV8842

Other Parts Discussed in Thread: DRV8871, DRV8842

Dear Motor Drive Team.

I have a question related to overcurrent protection feature in DRV8871: can it be assimilated to the one implemented on DRV8842 (on each fet) or is it monitored on the entire HB?

here below from DRV8842 DS

An analog current limit circuit on each FET limits the current through the FET by removing the gate drive. If this

analog current limit persists for longer than the OCP time, all FETs in the H-bridge will be disabled and the

nFAULT pin will be driven low. The device will remain disabled until either nRESET pin is applied, or VM is

removed and re-applied.

Overcurrent conditions on both high and low side devices; i.e., a short to ground, supply, or across the motor

winding will all result in an overcurrent shutdown. Overcurrent protection does not use the current sense circuitry

used for PWM current control, and is independent of the ISENSE resistor value or VREF voltage.

Furthermore is there any difference between the two DRV in terms of overcurrent protection in case of phase short condition?

Thanks for your inputs
Kind Regards

Nicola