This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8432 Schematic reveiw

Other Parts Discussed in Thread: ISO7242C

Dear MDBU expert,

Could you please help review the schematic design of DRV8432? thanks.

DRV8432_schematic_board.pdf

Best Regards

Iven Xu

  • Hi Iven,

    What is the application?

    Please see comments below:

    1) What is the PVDD voltage?
    2) Please check VCC2 connections on U102 and U103. D+12V violates absolute maximum voltage of the device.
    3) It appears ISO7242C is the correct device for U103. Please confirm.
    4) R104 should be 1Ohm, not 1kOhm.

    Please make sure the GVDD/VDD supply meets the requirements of section 8.2.1.2.2 Current Requirement of 12-V Power Supply
  • Hi Rick Duncan,

    Thanks for your reply, it is for medical application.

    I will double check with engineer for the PVDD and will back to you soon. thanks.

    Best Regards

    Iven Xu