This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BLDC kits

Other Parts Discussed in Thread: DRV11873, TIDA-00735

Can anyone suggest an EVM kit for a 12 V BLDC sensorless motor  which has very low inductance and 30k RPM?

I want to design an application where the fan regains its speed in case I obstruct it from running for a moment and then remove the object. I see several kits available, but I am unsure which one to try out first. 

I am considering the DRV11873 kit, but I wanted to make sure that the control is closed loop and that the motor will not stop completely after applying load to it.

Thank you.