Is use of current shunt ampilfier is necessary to use DRV8301 in OCP current limit mode?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is use of current shunt ampilfier is necessary to use DRV8301 in OCP current limit mode?
Then why my IC is not working in OCP current limit mode??????????????????????????????
It works only when i disable the OCP mode.
my device work in report only mode with nOCTW remains low.
In current limit mode whenever input PWM signal changes state nOCTW goes low for a very short time(I think 64us).Otherwise it stay high.
One more thing, my device work in current limit mode for HIGHER Vds threshold value such as 2.131V and 2.400V (set by SPI).So I think my device encounter overcurrent event in the lower Vds threshold values.But i don't know WHY?
I solved the problem by removing the gate resistance of the MOSFETs.Gate resistance reduces the switching speed of MOSFETs.
Due to gate resistance Vds sensing starts before completely TURNING ON the MOSFETs.So,before turning ON the MOSFETs Vds was 1.32V.So, Thats why my device work for higher threshold values such as 2.400V.
But, When i attache motor with the 3-phase bridge, device again encounter an overcurrent event like before.If i attache resistors with the 3-phase bridge than my device works properly.It means at the starting moment may be motor takes large amount current.
one more thing i wanted to know........
In OCP current limit mode, after enabling the MOSFETs how much time does DRV8301 takes to start Vds sensing???
If i know this than i can select proper gate resistances and MOSFETs for my project.