This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8801A-Q1 Use as a half H-bridge driver

Other Parts Discussed in Thread: DRV8801A-Q1

Hi Team,

Is it possible to use the DRV8801A-Q1 as a single ended driver without creating diagnostic fault codes or losing functionality?

Thank you,

Jared

  • Hi Jared,

    We will have to check, but in theory it is possible.

    To confirm, please answer the following questions:
    1) will the motor voltage be present before or after the DRV8801A-Q1 VBB voltage?
    2) how are the inputs being controlled? (PH/EN/MODE1/MODE2)

    Some of the bridge control cannot be used when the motor is configured this way.
  • Hi Rick,

    1) will the motor voltage be present before or after the DRV8801A-Q1 VBB voltage?

    I am not sure yet.. What are the consequences if the motor voltage is present before the DRV8801A-Q1 voltage?

    2) how are the inputs being controlled? (PH/EN/MODE1/MODE2)

    The inputs are being controlled from an MCU. Do you know specifically which aspects of the bridge control cannot be used when configured this way?

    Best regards,
    Jared
  • Hi Jared,

    Jared Becker said:
    1) will the motor voltage be present before or after the DRV8801A-Q1 VBB voltage?

    I am not sure yet.. What are the consequences if the motor voltage is present before the DRV8801A-Q1 voltage?

    That is one item we must check.

    Jared Becker said:
    2) how are the inputs being controlled? (PH/EN/MODE1/MODE2)

    The inputs are being controlled from an MCU. Do you know specifically which aspects of the bridge control cannot be used when configured this way?

    There may be other conditions, but ENABLE = 0, MODE1 = 1, and MODE2 =0 results in current flowing through the motor (low side slow decay). This condition should be avoided.