This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
The customer is using LM629M-6.
PIN 13(PWM MAG) can output PWM and PIN 11(PWM SIGN) is a low level occasionally when the board is power on without any initialization. The PWM for PIN 13(PWM MAG) is about 3%. The malfunction has appeared on several boards. Once this malfunction occurs, the motor rotates fast.
The attached are the schematic and the waveform for the malfunction. VCC is 5V and fCLK is 6MHZ.
What is the reason? How to solve the issue?
Thanks,
Best Regards,
Hello Mickey,
I have began to look into your issue and would like more information. You mention that there is a malfunction but what exactly is the problem? The PWM MAG is about 3% but what did you expect it to be? You also mention this malfunction occurred without initialization? It is important for the device to be initialized properly before operation. Please describe what you are intending to do to with this device so we can determine how to correctly accomplish that. Thank you!