Dear sir,
My name is Ketan
I had made one DC motor driver project using lmd 18200 t ic with arduino mc. My program is so simple and working fine. My motor is brushed 24 v DC .
Program is motor fwd and reverse control by two buttons no nc type. Pwm is only 10 period of 5 sec.
Motor rotate fine but with ought load.
If I putting on belt. Tensions it can not rotate.
Pls suggest me the solution
Thanks