This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

drv8302

Other Parts Discussed in Thread: DRV8302

Iam using drv8302 to run the BLDC motor.When i run the motor without any load the current in the drv8302 is about 4.8mA but as i increase the load on the motor the current in the drv8302 increases.It goes to 8mA when my motor current is 12A.

Is it a normal behaviour of drv8302 or something is wrong??

And what is the maximum current is allowed in the drnv8302 in proper working conditions??