This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What BLDC motor drive should I use?



Attached is a curve of the 3 phase BLDC motor I am trying to drive. I would like to have a supply voltage, to the driver, of 115vAC and the ability to control the speed/power supplied to the motor.   What BLDC motor driver should I select?

  • You may use an isolated AC/DC converter and produce 28Vdc bus voltage. Then you may use DRV8301-8302.
    Second method you may rectify the AC voltage with bridge circuit or PFC. Then you may use and IGBT module with integrated gate driver and digital isolation circuitry.