Hello,
I am looking for an evaluation board that can be used for regeneration in ebike.
I am using a bldc hub motor.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Mohit,
What is the maximum battery voltage when fully charged? The margin could be reduced significantly if the fully charged battery is ~56V.
One of the applications of the DRV8301-HC-C2-KIT is E-bike.
The DRV8301 has a recommended maximum voltage of 60V and absolute maximum voltage of 65V.
Hello,
Do the kit that you suggested work during regeneration?
Max battery voltage is 48V.
Thanks
Hello,
I read details about DRV8301-HC-C2 kit. This kit has C2000 Piccolo F28035 MCU controlCARD that helps to control the motor speed. Is that possible to change the control card in this kit. IS there any control card that can help in position and speed control both.
This kit has sensorless trapezoidal commutation can it be done by sinusoidal commutation.
As the controlcard comes preflased, using GUI it is not possible to control the position of the motor. So, is it possible if i load my own program in the control card. If yes how it can be done?
Thanks
Mohit