Hi! Is it possible DRV8711 to drive unipolar stepper motor?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Pavlin,
Yes, you can potentially drive a unipolar stepper motor with the DRV8711. For unipolar steppers, I would also suggest you take a look at the following devices: DRV8803, DRV8804, DRV8805, and DRV8806.
Ok, but hold on for second! In the AN Rick suggests there is a schematic where the voltage on DRV8711 is decreased to 12V. The DRV8711 says it can run up to 58V. Do I always have to decrease the DRV8711 supply voltage to 12V and use the original voltage to drive the bridge?
Thanks!