Hi
I've been trying to use the EVM with a DC motor or with a stepper motor (connecting it to both AOUT and BOUT) but failed to make them work.
I see the AENBL pin go high (or pulses on the STEP when working with a stepper motor) but the motor won't move. When using the DC motor, it seems to work when connecting it directly to DC but it didn't work using the DRV8834. I've connected a probe to AOUT1/2 but couldn't see and voltage on these pins. I double checked the configurations of AVREF and BVREF
Can someone please help?