This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069 / DRV8312 demo



Hello team,

Hope you are well.

A customer is looking into with driving the encoders with a BLDC motor.

This is a sensor-less sinusoidal commutation is desired, Current drive < 2A, rail at 24V. ( L= 48 mH and R= 48.9 ohms)

They are currently use a TMS320F2809 but are interested in the TMS320F28069 / DRV8312 using Instaspin support.

The goal is to support Position and Velocity control.  eQEP (2 Ch) is essential.

Is there a demo available and/or what information do we have that can help?

Regards,

Randhir