Other Parts Discussed in Thread: DRV2700
Hi Team
could you please have a look at my questions below?
1- We have to drive a 3.3uF 0V-150V piezo, at 15 to 20 Hz, positive sinus (or trapezoidal). Do you see a problem to achieve this with this chip and eval board ?
2- Do you have an estimation of the heat power dissipation on this driver in this configuration ?
3- In the case we would like to modify the reference flyback design in order to supply the current to the piezo from a 12V source instead of a 5V source, do you have a suggestion for the required modifications? Is this possible?
Best regards
SF