This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FAULT always LOW

Part Number: DRV8432


Hello,


Im trying to use DRV8432 as voltage inverter in paralell full-bridge mode (schema below).

When I apply 60kHz PWM at PWM_A or PWM_B the FAULT output is low. (GVDD is 12V and PVDD 20V) The output was mostly random noise.

Is some special startup sequence required (datasheet says it doesn´t)?

Thank you, Ondra.