This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I have an application were I need to switch very quickly from output to hi-impedance outputs. The DRV8837 seems to offer this.
Unfortunately the output current is not sufficient. I would like to connect the inputs and outputs of multiple of these chips together to boost the output current.
As the H-bridge consists of mosfets with a positive temperature coefficient they should share the current evenly.
Is this correct ?
My load is resistive.
Regards, Ruud