Hi,
I'm trying to use a DRV2603 to control a C10-000 LRA from Precision Microdrives (www.precisionmicrodrives.com/.../c10-000-10mm-linear-resonant-actuator-3mm-type) but the vibration is "weak" and the control signals don't look right when compared to the datasheet.
This is the circuit I'm using :
The three DRV_* pins are controlled by a microcontroller and driven to continuous 1. The application seems simple enough and I don't know where I went wrong. The motor manufacturer says this is a driver issue and that they don't know. I've built 3 prototypes, all of them had the problem, so this looks like a design issue.
Do you know where it could come from and how to fix it?
Thanks
S.