Hi,
I have designed a BLDC driver Board using DRV8301, all is working fine i am able to drive the Max or any BLDC motor successfully at a rate velocity and position etc.
I am able to ramp up and run and ramp down the motor successfully no issues till now. Now this issue is, its a circular devices that runs around the pipe the motor is fitted on it, drive is able to run the motor in circular position along the pipe and stop at a give angle degree on the pipe. But no the issue is when i had any load on the device and try to stop the device just slips to the bottom of the pipe i.e 180 degree.
How to solve this problem when there is a load applied, how do i hold the device at say 90 degree with 20kgs of load, without slipping,
Is there any breaking mechanism that i can adapt please guide.
Regards
Mahesh Prasath.