Hi, I tried to change my DRV8303's pwm_mode to 3-pwm input via SPI
It successed on read/write 0x0-0x3 but only PWM_MODE, once I set to 3-pwm input that next cycle gives a fault bit.
could any reason causes this case like me? Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, I tried to change my DRV8303's pwm_mode to 3-pwm input via SPI
It successed on read/write 0x0-0x3 but only PWM_MODE, once I set to 3-pwm input that next cycle gives a fault bit.
could any reason causes this case like me? Thanks!
Part Number: DRV8303
Hi, I tried to change DRV8303 'PWM_MODE' to 3-pwm input,
I do access 0x00-0x03 registers via SPI well but once I change register 0x02 D3 as 3-pwm input
It responsed a fault bit(F0), any reason could cause case like me? Thanks!