This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8711: Using Multiple DRV8711 -- Connect V5 outputs for additional current

Part Number: DRV8711

I am using 4x DRV8711 for a 4-axis CNC application.

I would like to utilize the 5V LDO internal to the DRV8711 (V5 pin) to supply the power for the rest of the system, including MCU.  However, the 10mA limit may be a bit restrictive.  Is there a way to connect all four V5 outputs, to get 40mA effective current?  Obviously I would want to avoid backpower -- perhaps a 'diode-ORed' solution?