In page 10, it is written that the maximum allowed resistor for current limiting is 1 Ohm. (Which is a bit different than what I find in other DRV88x family datasheets.)
We need to detect 100 mA as Trip current, It means I need to place a 2 Ohm resistor. (Not allowed by the datasheet).
How can we do so ?
Maybe it is a datasheet mistake ?
(I Think there is something wrong with this line as it also says that I can current limits higher than the device maximum rating.)
Maybe a different driver ?