This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8844: 4ch low side switch

Part Number: DRV8844

Dear Support team,

 

Is it possible to use DRV8844 as 4ch low side switch?

In that case, should we connect directly SRC12 and SRC34 to GND?

Are OCP function individually available for the each channels?

 

Best regards,

Hiro Takahashi

  • Hi Takahashi-san,

    Yes it is possible to use the DRV8844 as a 4ch low side switch.
    You can connect SRC12 and SRC34 directly to VNEG if current monitoring is not required.
    OCP are individually available for each channel. Please refer to section 7.3.5.1 of the datasheet for details.