I am trying to use this board to drive a brushless 3-phase dc motor. I am supplying the board with ~12V of power in and the power LED is on. The motor I am driving will pulse 3 times followed by a pause and then 3 more pulses. This pulsing pattern repeats indefinitely. Any idea as to why I can’t seem to get the motor to drive continuously?
Power source:
https://www.amazon.com/T-Power-12V-1-5A-Power-Adapter/dp/B009ZZFMSQ
Motor:
https://www.precisionmicrodrives.com/product/912-101-12mm-brushless-vibration-motor-15mm-type