Hi SIrs,
We would like to know if there is any bit address can be revised for the vibrator be shaking or quiet alternatively in analog input mode. The vibrator is always shaking when customer put the a long period analog signal into the pin B1.
Example:
Analog input Amplitude>0.9V, DRV2604 shakes the vibrator
Analog input Amplitude<, =0.9V, DRV2604 stops shaking the vibrator
Thank you and Best regards,
Wayne Chen
01/20/2017