Other Parts Discussed in Thread: DRV10983, MSP430G2533, MSP430G2553, USB2ANY
Tool/software: Code Composer Studio
I am new to this field and am learning to use the Target board and Launchpad to program DRV 10983. I have a motor spinning successfully and am wanting to program the 10983, with program data from the EVM , using the Target board plugged on to the Launchpad.
Guidance i need is in matter of how to transfer the file saved from the GUI to Register_Values.h' with the register values entered as is suggested in para 3 of Targetboard programming guide. I am not able to follow and use the following instruction. quote........
Figure 12. Example Register Settings Entered into the Programming Tools Code
3. Define the register values in the programming code to match the tuned values from the GUI. The
downloaded project has the registers defined in ‘Register_Values.h’, but these need to be changed to
the tuned values from the GUI. As shown in Figure 12, the defined register values in the code (right
side) need to match the registers in the file saved from the GUI (left side). To open
‘Register_Values.h’, expand the project in the project explorer window and double click
'Register_Values.h'. Manually enter each register value from the GUI file into the program code. Make
sure to save ‘Register_Values.h’ after the new register values are entered.
..................unquote
I would be obliged if someone on the forum can guide me.