This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10975EVM cannot update

Other Parts Discussed in Thread: DRV10975EVM, USB2ANY

Dear,

During using the part #DRV10975EVM, tried to connect with HPA665 board.

But it can't pass and the firmware needs to update message popped up as below.

The connected <unknown device> requires a firmware update to version 2.6.3.0.

Serial Number: A2EA986F03000F00

Current version: UNKWON

The update takes only a few seconds and does not require an Internet connection.

I checked this message but cannot use it still. Please advise how can it update.

Thank you