This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SRM Motor Control

Hi All ,

i am new to SRM motor control...

i want to control a 1KW SRM motor .

The specifications are

Motor Power -1Kw

Supply Voltage -230V AC

Speed -150 RPM to 12000RPM

Torque - 60Ncm@12000RPM, 6Nm @150RPM

The Speed need to be controlled from 150 RPM to 12000RPM. 

what is the position sensor i need to use to commutate the motor. please provide any reference electronics design. i know the h bridge used for this is bit different from BLDC motor Control. so how my H bride Design and its gate drive design need to be done.

please provide what is the commutation sequence i need to use.

is there any reference schmatic ?

thank you...