This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8812: Risense of DRV8812

Part Number: DRV8812


Dear Sirs,

My customer asked us about Risense of DRV8812.

Customer is measuring Ichop by changing Risense from 0.5 Ω to 0.68, 0.47.
So setting current regulation to 38% with this setting will result in a value different from the calculated value of the data sheet formula.
Please let me know if there are restrictions on the Risense.
When Risense = 0.47 Ω, the waveform of the output current is also disturbed.
Please also tell me about this cause.

Best Regards,

Y.Hasebe