This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10975EVM: USB2ANY damaged MCU

Part Number: DRV10975EVM
Other Parts Discussed in Thread: MSP430F5529, DRV10975, USB2ANY,

Hello to all,

I started to develop BLDC motor pump controller using DRV10975 chip and purchased development kit DRV10975EVM. It was no problem to play with this kit, but after some time I accidentally connected 12V to I2C line from DRV10975 to USB2ANY and damaged its MCU MSP430F5529. I´ve desoldered damaged one and soldered new one and tried to load firmware using USB2ANY Firmware Loader. When I press USB2ANY button to start bootloader, I can see one device in available devices, it is displayed as Type: No Firmware, Serial Number: Unknown, Firmware ???, Driver HID(BSL). When I try to update firmware, all seems to upload firmware and firmware loader ends with message USB2ANY firmware update is complete. Seems well, but it isn´t. USB2ANY is not recognized by DRV10975 EVM GUI or USB2ANY Explorer. Is there any possibility to reprogram new MCU to fix USB2ANY to be working again?

Thank you and Best Regards

Michal