This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8711: Used as a stepper driver for cnc without SPI

Part Number: DRV8711
Other Parts Discussed in Thread: DRV8308,

Hello!

I am working on a stepper driver compatible for a PCB milling CNC machine.

The question i wanted to ask is regarding the motor enable. From what i understand, the "enable motor"   feature is available only over spi by writing bit0 in register 0x0h. The problem is that i need a physical parallel command to enable the motors.

My only thought of a solution is to use a small uC to send the SPI data only once at powerOn and use the SLEEPn pin as the ENABLE.

Is there any other or easier solution for that? i worked in the past with the DRV8308 and the chip had a "memory save" function which would have been great here, but the datasheet does not say anything about this for the DRV8711.

Thank you in advance!