Part Number: DRV8432
Dear Technical Support Team,
Could you tell me the peak current condition on datasheet?
for example,
DRV8432(8412) can drive peak current under 1msec or Duty is under 50% and so on.
Otherwise, Is it no problem that temperature is under the recommend operation range?
■datasheet
• DRV8412 (Power Pad Down): up to 2 × 3-A
Continuous Output Current (2 × 6-A Peak) in Dual
Full-Bridge Mode
• DRV8432 (Power Pad Up): up to 2 × 7-A
Continuous Output Current (2 × 12-A Peak) in
Dual Full-Bridge Mode
Best Regards,
ttd