This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV11873: What is meant in datasheet by "high speed" application?

Part Number: DRV11873

In section 9.2.2 of the TI DRV11873 datasheet is states:

– If the motor is high current / high speed, use three Schottky diodes between the phases and ground.

What is high current?  

What is high speed?

I ran chip at 14V to drive a 3 phase motor with speed constant of about 1000 RPM/V without the above mentioned Schottky diodes.  Motor was drawing < 0.6A.  

IC failed.   PWM input is now pulled to +5V always by the DRV11873 IC.  Did failure to use the three Schottky diodes cause this? 

Thanks,

Dave

  • I should have also mentioned that motor was run at 6000 RPM
    - Dave
  • Dave,

    You will need to do more lab work to figure out what was the root cause of the device failure. Schottky diode recommendation is to prevent phase voltage going below - 1 which is the abs min of DRV11873. When there is much current on the phase and driver goes into tri-state period, we can see phase voltage is below negative.

    The best way is to monition phase voltage and if it goes below -1, you will need to place schottky diode.

    Thanks,

    Seil