This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8825: RMS output current for DRV8825

Expert 2415 points
Part Number: DRV8825


Hi Ti,

Referring to the DRV8825 datasheet, max RMS output current applied to each winding is 1.75A rms or 2.5A peak.

The max 2.5A peak is it refer to only positive or negative current of one of the motor winding measurement as below?

Is measurement below with 1.36A peak current which is within DRV8825 2.5A peak spec?