Other Parts Discussed in Thread: DRV10983
Dear whomever it concerns!
From the display tab I can monitor the motor velocity constant.
When running at no-load the constant is almost constant across the possible speed range.
Applying a load like a fan wheel that creates a load that increases with speed.
Increasing the shaft load from noload will lower the speed but now also significant change in the velovity speed constant.
What velocity constant should I use in the application?
The constant at full load and full speed or something else?
From the SLOU395C I can not find any advice regaring this.